Hi @matt-crc,
There is no internal pull-down resistor on this pin.
Note: The connection schematic of VDDA18PMU and VDDSMPS on this board does not exactly match the recommendations in AN5967 (Figure 4: System supply configurations) because the STM32N657-DK board was designed much earlier than the application note.
You can refer to application note AN5967 section 3.7 System startup and the Datasheet DS14791, specifically section 3.4.4 SMPS usage, which provide guidelines to follow for using the SMPS.
When the design is in SMPS Bypass mode (SMPS disabled), VDDA18PMU, VDDSMPS, and VFBSMPS must be connected to ground (GND) to prevent them from floating.
Thanks.
ELABI.1