STM32U5 UART - loopback test
Hi! I have a STM32U585 board and I'm trying to make a UART loopback test. I tried two different modes:
- Asynchronous (Full-Duplex) - wire between the TX and RX
- Single-Wire (Half-Duplex) - wire looping to itself
Both worked in similar ways. I successfully was able to handle 1 byte, so this is the code that worked fine
/* USER CODE BEGIN PV */
uint8_t tx = 0;
uint8_t rx = 0;
/* USER CODE END PV */and inside the main function I had
while(1)
{
printf("Sending byte: %d\r\n", tx);
HAL_UART_Transmit(&huart3, &tx, 1, HAL_MAX_DELAY);
HAL_UART_Receive(&huart3, &rx, 1, HAL_MAX_DELAY);
printf("Received byte: %d\r\n", rx);
tx++;
HAL_Delay(1000);
}I could see in the terminal that it was successfully incrementing both tx and rx variables.
Now, it all went wrong when I tried to use an array instead of a single byte. This is what I tried:
/* USER CODE BEGIN PV */
uint8_t tx[4] = {0x55, 0x12, 0x00, 0xFF};
uint8_t rx[4] = {0};
/* USER CODE END PV */and the main function had
while(1)
{
printf("Sending bytes:\r\n");
for(int i=0; i<4; i++)
printf(" 0x%02X", tx[i]);
printf("\r\n");
HAL_UART_Transmit(&huart3, tx, 4, HAL_MAX_DELAY);
HAL_UART_Receive(&huart3, rx, 4, HAL_MAX_DELAY);
printf("Received bytes:\r\n");
for(int i=0; i<4; i++)
printf(" 0x%02X", rx[i]);
printf("\r\n");
tx[2]++;
HAL_Delay(2000);
}From this in the terminal shows that it got stuck at HAL_UART_Transmit(), this was the full output
Sending bytes: 0x55 0x12 0x00 0xFF
By running it in debug mode I was able to realize that it got stuck on this while loop inside the stm32u5xx_hal_uart.c
HAL_StatusTypeDef UART_WaitOnFlagUntilTimeout(UART_HandleTypeDef *huart, uint32_t Flag, FlagStatus status, uint32_t Tickstart, uint32_t Timeout)
{
/* Wait until flag is set */
while ((__HAL_UART_GET_FLAG(huart, Flag) ? SET : RESET) == Status)
{
...Can anyone help me out? Is there any info about my test that you need me to provide?
Thanks in advance!