STM32U585 memory mapped hyperRAM and STOP2
I'm using a STM32U585 that has some hyperRAM attached to OSPI2. I've memory mapped it and it's working well during normal operation. I've noticed, though, that when I leave it powered and put the processor into Stop 2 mode, it corrupts some of the data in the hyperRAM after I come out of Stop 2 and re-configure the clocks. It doesn't happen every time.
Should I be re-configuring the Hyper Bus after I come out of Stop 2 as well? Is there any known reason to be cautious about using the Stop modes while the OSPI is being used for memory mapped external memory?