STM32U5G7VJT6Q GPIO Input issue
Hi,
I'm using the STM32U5G7VJT6Q microcontroller to read input from a few switches. All switches should show a high state when unpressed (due to the pull-up resistor) and a low state when pressed (grounded).
However, one switch is acting strangely:
- When it's unpressed, it stays in a low (reset) state, but it should be high.
- It only changes to high when another switch is pressed.
- The other switches are working fine.
- The switch is connected in the following order: TVS diode -> Pull-up resistor -> RC filter -> GPIO pin.
- The GPIO pins are set as inputs with internal pull-ups enabled.
- The wiring looks correct, and the pull-up resistor is in place.
- The other switches behave as expected.
- Tried removing the tvs diode and capacitor in rc as well, still the same behavior occurs
Note: No input of the switches are shorted or grounded, the behavior is observed in all the boards we fabricated.
Questions:
1) What is the possible cause for this behavior?