STM32U5G9J-DK1 demo project
I plugged in the microB cable only to power demo board STM32U5G9J-DK1. Now the LCD on it display different images in certain sequence. Firmware package STM32Cube_FW_U5_V1.7.0 has been downloaded. I assume the demo project is the DSI example folder. \STM32Cube_FW_U5_V1.7.0\Projects\STM32U5x9J-DK\Examples\DSI
There are two examples. Which one should be the one that was loaded into the demo board?

My application is to send videos through the USB C port and display the video on the LCD display. In this case, if there is an example firmware and example software to evaluate, it would be very helpful.
Thank you.
Kelly