SWD connect frequency decreasing after initial programming
On a custom board, we have an issue where after our first connection at 8MHz over SWD, then programming, we can only connect at 50kHz or slower. Has anyone seen this before? Could there be an issue in our hardware design/layout that is causing the connection to be so slow? Or something in our firmware configuration? It seems like it is likely in the configuration somewhere. If we erase the chip an program on a different program, it seems ok, but still baffled what could be wrong in the firmware config.