Switch Between DFU and User Application in Software (NO Physical Interaction)?
Hello team,
I’m working with an STM32H745iik6/ Nucleo-H745ziq microcontroller and currently using USB DFU mode to upload firmware. The process involves setting BOOT0 to 1 and performing a manual reset to enter DFU mode. After uploading the new firmware, I manually set BOOT0 back to 0 and reset the board again to run the user application.
otherwise any ST software like stm32cubepgm to select DFU mode or user_apllication mode?
Current Approach:
- Enter DFU Mode:
- Set BOOT0 to 1.
- Perform a manual reset.
- Upload Firmware via USB DFU.
- Run User Application:
- Set BOOT0 to 0.
- Perform another manual reset.
Goal:
I want to automate this process entirely through software without the need for physical interaction. Specifically, I’m looking for a way to:
- Switch to DFU mode using software.
- Upload new firmware.
- Automatically return to the user application after the firmware upload.
- Is it possible to switch between DFU mode and the user application purely through software on STM32 microcontrollers?
- If so, can someone provide an example or detailed steps on how to achieve this?
- What are the best practices to ensure a smooth transition between DFU mode and the user application without manual intervention?