Switched my STM32F4 discovery and now Virtual Com port is not working
Hi,
i swapped my first STM32F407G-DISC1 discovery board for a new one and now the ST-Link onboard doesnt show up as a virtual com port in Windows 10 anymore.
I flashed the St-Link with the new firmware, it runs V2.J30.S0 STM32 Debugger now.
I also installed the current Windows driver from
.Now i read the DISCOVERY boards dont all have the virtual com, but in
http://www.st.com/en/evaluation-tools/stm32f4discovery.html
it says that my order code should have it (on my PCB is a silk print next to the USB connector that says 'STM32F407G-DISC1).Can it be that the silkscreen board code doesnt correspond to the 'order code' which is mentioned on the above website?
Please help since i really need the virtual COM port.
Patrick
#st-link-v2-1 #stm32f746-discovery #stm32f4