Question
Synchronizing 2 timers for PWM input ?
Hello,
Is there a way to synchronize 2 timers in PWM input so that the second timer will do the PWM input reading in sync (in phase) with the first (master) one ? I see that it is possible with PWM output but for PWM input the "trigger source" is grayed out in CubeIDE.
I'm using the H723ZG 144-Nucleo board.
Thank you, J.