T_VCC on STLinkV3 vs VCC on target
I have made an adapter that sits between the STLink V3 and the device that needs to be programmed, so that I can give T_VCC on the STLink side 3.3V from an external supply.
So far I have used 3.3V as VCC on the target as well, but I am considering lowering VCC on target to 3.0V instead.
As far as I can tell from datasheets, there shouldn't be an issue with keeping T_VCC on the STLink side at 3.3V while VCC on target is 3.0V, but I wanted to check here if anyone has something different to say about this mismatch.
If it's a bad idea, I will need to have adapters around with T_VCC 3.0V and others with T_VCC 3.3V depending on which target device I work with, which in this case is a bit of a hassle.