Technological for soldering question
We plan to use in one of our products WLCSP49 package.
Please see page 126(PDF attached) - According to Table 80. "WLCSP49 recommended PCB design rules (0.4 mm pitch)" , the recommended Dpad Dimension is 220 µm.
We perform some measurements on the PCB and found out that The actual Pad size is between 178-192 µm.
· Do you have any recommendations for the stencil in this case?
· Are we going to face with reliability problems?
· What is the minimum Dpad Dimension that allowed?
Thanks
Roni