The STM32H757I-EVAL is compatible with STM32H757BIT6
Hi,
I'm planning to start a project with the STM32H757BIT6 microcontroller (MCU). I'd like to use the STM32H757I-EVAL evaluation board, but I noticed it utilizes the STM32H757XIH6 MCU.
I'd like to confirm if I can begin development using this evaluation board. While I understand the STM32H757XIH6 MCU may have additional pinouts, is the STM32H757I-EVAL still compatible with the STM32H757BIT6?
Can I start my project using this evaluation board and after my prototipe is done, change simply configure it for the new target MCU? Of course, I'll need to be mindful of only using the pinouts available on the STM32H757BIT6.
Thanks!