Question
This is a question regarding STM32 crystal and Load CAP(2)

Data for the parts used are shown in the photo above.

I made the calculation as above, but I am curious as to whether I obtained the CL value correctly.
result)
→ECS-.327-12.5-12R-C-TR (32.768kHz CLoad 12.5pF, Cs 5pF)
CL1=CL2=(CLoad-Cs)*2=(12.5pF - 5pF)*2
CL1, CL2 →15pF (14~16pF)
→ECS-120-8-36-CKM-TR (12Mhz CLoad 8pF, Cs 5pF)
CL1=CL2=(CLoad-Cs)*2=(8pF - 5pF)*2
CL1, CL2 →6pF(5~7pF)