Trouble Using An External Programer with Nucleo-G031K8
Hey, I'm using a NUCLEO-G031K8 board. I currently have jink running on it, and I can easily run debug and program with the USB interface. I'm currently trying to flash it using an external jink EDU programmer, and I have also tried by buying a larger NUCLEO Board and snapping off the programmer to program it. All these seem to connect to the NUCLEO, but they all error when they try to erase the board.
Do I have to connect Solder bridge 2 (st-link reset).
Or is there another Configuration I have to do with the hardware?
I have already soldered on the 5 programing pins, and also edited the NRST register so that it is not acting as a GPIO pin.
any help would be gladly appreciated.