Trouble with configuring CTC for STM32F303ZE Nucleo board
Hi,
I did the basic set up for configuring the usb micro A device connector added on the nucleo board (not the ST-Link connector). Clock is set for usb (HSE, 48MHz through PLL) and the USB_VIRTUAL is set on CTC.
I generated the code with Cube IDE and pushed it... and nothing. When I connect both usb (ST-Link and Virtual COM), my computer only sees St-Link.
Im I missing something? Is there a jumper to change place to active the second usb connector?
Thanks!