Skip to main content
Visitor II
January 27, 2022
Question

Turn off SMPS STM32U585AII6Q

  • January 27, 2022
  • 4 replies
  • 1605 views

Is it possible to turn off SMPS in ST​M32U585AII6Q and not to use external inductors and capacitors needed for SMPS?

Thanks in advance,

Nenad​

    This topic has been closed for replies.

    4 replies

    Super User
    January 27, 2022

    Yes. The chip uses LDO by default. If you don't want SMPS, don't switch to it.

    Visitor II
    January 27, 2022

    Most low-power-conscious power supplies have power-saving features included, similar to what you have described. There are some considerations to keep in mind.

    Super User
    January 27, 2022
    In this case, SMPS is the power saving option compared to LDO.
    NGajicAuthor
    Visitor II
    January 28, 2022

    0693W00000JNepVQAT.pngOk, so do we need to do something in hardware or software to set usage of LDO only? Can we leave VLXSMPS and V11 pins unconnected? On ST evaluation board B-U585I-IOT02A they connected those pins as shown in the picture in attachment.

    Thanks in advance,

    Nenad

    ST Employee
    February 4, 2022

    Dear Nemad,

    To clarify a bit your statement,

    On a given board set for SMPS, LDO option can works (and is the default start up mode in fact).

    But if you don't consider using the SMPS at all, the self can be drop on your HW, not the capacitor however which are required on LDO V11 pads.

    Best regards,

    Antoine