Two boards STM32H757I-EVAL seem dead after USART1 (CN2) to RS232 connection
Hello
I got two boards dead within one day. I used the first board for a while and it worked until I started to communicate via USART/RS232. After I faced with such a problem, I replaced the board with a second one and immediately got same result.
Description:
The eval board was powered via STLINK-V3E USB (CN23). JP10 in corresponding position, no other jumpers are reconfigured. No connection to RS232 at the beginning. LCD display showed a nice picture, IDE successfully uploaded and debugged both M4 and M7 etc.
Power off and on at least with the first board did not change the situation as well.
Then I connected it to a PC com port (USART1 via CN2). To do that I used a USB to COM convertor from StarTech.
At the beginning of debugging I got in a PC terminal:
"STM32H747I-EVAL: STFirmware (Fractal) V1.0.0 (Build Feb 8 2019 at 19:22:02)
CPU running at 237MHz, Peripherals at 118MHz/118MHz"
and then my own prints and readings.
Then the story with two boards a bit differs. For example, with the second board I very quickly (in couple of minutes) faced with USART malfunction. It became unable to transmit. Or transmitted just couple of chars I wanted and got stuck.
Anyway, once I turned the board off and then turned on again - no LCD picture and no ability to upload and debug the executables. With the second board and with the first. Both today.
"Target no device found
Error in initializing ST-LINK device.
Reason: No device found on target."
"Error in final launch sequence:
Failed to start GDB server
Failed to start GDB server
Error in initializing ST-LINK device.
Reason: (4) No device found on target."
That happened with two boards in turn.
Besides, I tried to use STM32CubeProgrammer utility. It says that on-board ST-Link programmer is not able to detect the target MCU.
Your comments?