UART signal on SWO pin from ST-Link V2/3
Hi
For a project, we have switched from a M3 to a M0 microcontroller, which lacks the SWO that we used in production. We now want to connect the SWO pin of the debug connector to UART TX and use an external adapter to read it out. My question is, what would happen if we connected the debugger (ST-Link V2/3) without the adapter and the SWO trace received a (3.3 V) UART signal? Would there be a problem with the debugger?
Best regards, Mathieu