UART using st-link v2-1 break up from Nucleo F446RE
Hello,
the UART is not working.
st-link is stand alone (not connected to Nucleo anymore)
i am using a separate stm32f446ret6, tx(PIN16) and rx (PIN17) are connected to CN3 (TX/RX).
in addition the SWD CN4 of the st-link is used (all connections are made to the uC).
Programming is working fine. COM port is shown once i connect the st-link but tera term is showing nothing.
going back to a second board where the st-link is still part of the Nucleo (not break up) everything is working, uart is working.
What do you need to know to support me?