Unable to connect BlackPill via ST-link
Hi,
When trying to connect the board via ST-link in CubeProgrammer i get the error: "No STM32 target found!..."; can't figure out what problem is preventing ST-link from finding the target.
BlackPill is working properly, i can use it via DFU, but I would like to use debug.
I tested the ST-link dongle with a NUCLEOF303RET6 and it works fine.
Then i tried using the onboard ST-link of the NUCLEO to connect the BlackPill (with the correct configuration) and had the same problem; so i think the problem may be in the BlackPill (could it be an incorrect code in the identification registers?).
I also tried different bootloaders, although i don't think they can make a difference in this case.
Board: WeAct BlackPill V3.0, MCU: F411CEU6 (original), SWDIO and SWCLK correctly configured on pins PA13 and PA14 (SWD configuration), target voltage 3.28V.
ST-link: V2 dongle, MCU: F103C8T6 (original), tried with reset pin connected, tried with various firmware versions (now v2J45S7).
CubeProgrammer: no mode and reset mode works, tried various versions (now v2.17.0). (ST-link Utility too).

What am I missing?
Thanks for your time.