Unable to connect the external ST/Link V2 with NUCLEO-C031C6
Hello Team,
I am trying to use the external ST Link V2 with NUCLEO-C031C6,
Below are the connections,
1. I have removed CN2
2. JTAG Connections are below
1- MCU VDD to 3.3V pin of CN6
2. SWDIO - PA13 of CN7
3. SWCLK - PA14 of CN7
4. NRST - NSRT pin of CN6
5. GND - GND pin of CN6
6. GND(16)- GND pin of CN6
I have given 5V at JP5 pin, Able to see the MCYU get power at JP6
With this connection I am unable to program the MCU, getting this error

Please help on this