Unable to erase flash in NUCLEO-G0B1RE board
Hi
I am using the function below to erase the flash, but am not able to do the same.
I have to erase from address 0x0803E000UL i.e. page 124
The function does basically
1. HAL_FLASH_Unlock
2. HAL_FLASHEx_Erase(&erase_init, &page_error) - where page is 124
3. reads the erased flash area
4. HAL_FLASH_Lock
Am I missing something? I would not prefer to run the function in ram
I have MCUboot running and my application running on slot 0 is based on FreeRTOS. I am trying to erase slot1.
#define SLOT1_BASE_ADDR 0x0803E000UL
void erase_slot1_flash(void)
{
HAL_StatusTypeDef status;
uint32_t page_error = 0;
FLASH_EraseInitTypeDef erase_init;
uint32_t page_index;
/* Determine actual flash size (in KB) from system memory register */
uint32_t flash_size_kb = *(uint16_t *)FLASHSIZE_BASE;
uint32_t flash_start = FLASH_BASE;
uint32_t flash_end_addr = FLASH_BASE + (flash_size_kb * 1024UL) - 1UL;
printf("SLOT1_BASE_ADDR = 0x%08lX\r\n", (unsigned long)SLOT1_BASE_ADDR);
printf("FLASH_BASE = 0x%08lX\r\n", (unsigned long)FLASH_BASE);
printf("FLASH_SIZE_KB = %lu\r\n", (unsigned long)flash_size_kb);
printf("FLASH_START_ADDR = 0x%08lX\r\n", (unsigned long)flash_start);
printf("FLASH_END_ADDR = 0x%08lX\r\n", (unsigned long)flash_end_addr);
/* Sanity check: make sure SLOT1 lies within flash */
if ((SLOT1_BASE_ADDR < flash_start) || (SLOT1_BASE_ADDR > flash_end_addr)) {
printf("Error: SLOT1_BASE_ADDR is outside internal flash range!\r\n");
return;
}
/* Compute which flash page the slot address belongs to */
page_index = (SLOT1_BASE_ADDR - FLASH_BASE) / FLASH_PAGE_SIZE;
HAL_FLASH_Unlock();
printf("Before erase: ");
for (uint8_t i = 0; i < 16; i++) {
uint8_t val = *(uint8_t *)(SLOT1_BASE_ADDR + i);
printf(" %02x", val);
}
printf("\n\r");
/* Prepare erase configuration */
erase_init.TypeErase = FLASH_TYPEERASE_PAGES;
erase_init.Page = page_index;
erase_init.NbPages = 1;
printf("Erasing page (index=%lu, address=0x%08lX)\r\n",
(unsigned long)page_index, (unsigned long)SLOT1_BASE_ADDR);
/* Optional: clear prior flash flags */
__HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_OPTVERR |
FLASH_FLAG_RDERR |
FLASH_FLAG_FASTERR |
FLASH_FLAG_MISERR |
FLASH_FLAG_PGSERR |
FLASH_FLAG_WRPERR |
FLASH_FLAG_PROGERR |
FLASH_FLAG_OPERR);
status = HAL_FLASHEx_Erase(&erase_init, &page_error);
if (status != HAL_OK) {
printf("Erase failed! HAL status=%d Flash error=%lu\r\n",
status, HAL_FLASH_GetError());
} else {
printf("Erase successful.\r\n");
}
printf("-After erase: ");
for (uint8_t i = 0; i < 16; i++) {
uint8_t val = *(uint8_t *)(SLOT1_BASE_ADDR + i);
printf(" %02x", val);
}
printf("\n\r");
HAL_FLASH_Lock();
}