Unable to flash STM32F401RET6 from ST-Link Utility or STM32CubeIDE
I have successfully tested a prototype with the Nucleo F401 board and I have now moved the design to a custom PCB but I cannot program the microcontroller. The microcontroller STM32F401RET6 is not detected in the ST-Link Utility tool or in the STM32CubeIDE. The 3.3V is supplied to the MCU correctly. There are no peripherals connected to the board at the moment.
Did I miss any connection here?
I have tried these: connect VBAT to 3V3, changed C7, C8, C9, C10 to 100nF, changed C12 to 4.7uF for VCAP1.
The MCU is still not detected and I tried with my second board too. This rules out the MCU being broken.