Skip to main content
Visitor II
October 16, 2025
Question

unable to interface spi with stm32u5g9j-dk2 board

  • October 16, 2025
  • 2 replies
  • 335 views

I am working with the STM32U5G9J-DK2 discovery board and trying to interface an SPI peripheral

However, I am unable to get the SPI communication working.

I configured SPI in STM32CubeIDE but I’m not sure which SPI instance and pins are actually free to use. I suspect some pins are already connected internally to the LCD or Octo-SPI flash.

    This topic has been closed for replies.

    2 replies

    Super User
    October 16, 2025

    @vaibhavivele wrote:

    I’m not sure which SPI instance and pins are actually free to use.


    If you specify the board when you create the CubeMX project, it should identify which pins are used by on-board features.

    Otherwise, check in the User Manual for the board, and the schematics.

    The User Manual can be found on the 'Documentation' tab of the Product Page:

    https://www.st.com/en/evaluation-tools/stm32u5g9j-dk2.html#documentation

    and the schematics will be on the 'CAD Resources' tab:

    https://www.st.com/en/evaluation-tools/stm32u5g9j-dk2.html#cad-resources

     

    Graduate II
    October 16, 2025

    Hello @vaibhavivele 

    You can use the SPI1 interface on PA5 SPI1_SCK, PA6 SPI1_MISO, PB5 SPI1_MOSI and PB0 SPI1_NSS. They are all available on the CN4 Arduino connector of the boards (pins number 3 to 6).

    Best Regards.

    II