Unable to program the device. Error: Flash Download failed - Target DLL has been cancelled
I had my C code running on NUCLEO-F411RE last week. I downloaded it with Keil uVision and STLink driver. But, I did something when I tried to flash it today with an assembly code instead of the C code. Now, I cannot flash the device.
* A pop up window with the following message.
"No target connected. "
* I get another error message in the Build Output window.
Error: Flash Download failed - Target DLL has been cancelled
ST Link driver is still working. When I plug in the board, I get STMicroelectroinics STLink Virtual COM Port (COM15) in Windows' Device Manager. My Keil IDE can detect the board with the correct serial #. Last week, I had upgraded the firmware on the board through Keil IDE.
I tried to uninstall and install ST Link driver again. It did not fix the problem.
Could the boot load firmware have been corrupted?
Thank you for any help you can offer.
Michael