Unplugged target or STLink already in use or STLink USB driver not installed. System32 Workbench
Hi,
I am using STM32 Workbench with NUCLEO-H743ZI. The IDE is unable to connect to the board. I get the message Unplugged target or STLink already in use or STLink USB driver not installed. I have installed dpinst_amd64 from en.stsw-link009 and have tried different boards with different USB cables. I am running Windows 10.
How can I get the System32 workbench IDE to connect to the NUCLEO-H743ZI?
Here is the OpenOCD error details:
Unplugged target or STLink already in use or STLink USB driver not installed
Open On-Chip Debugger 0.10.0-dev-00015-gaaf1808 (2018-11-13-13:07)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
srst_only separate srst_nogate srst_open_drain connect_assert_srst
Info : The selected transport took over low-level target control. The results might differ compared to plain JTAG/SWD
adapter_nsrst_delay: 100
adapter speed: 1800 kHz
Info : clock speed 1800 kHz
Error: open failed (no matching adapter found)
in procedure 'init'
in procedure 'ocd_bouncer'