Updating the firmware of a X-NUCLEO-BNRG2A1 using the integrated ST-LINK V2-1 of a NUCLEO-L476RG
I'm having trouble updating the firmware of a X-NUCLEO-BNRG2A1 using the procedure described in AN5651 page 4 ("Direct update on the X-NUCLEO-BNRG2A1 expansion board" through the NUCLEO64-L476RG integrated ST-LINK 2-1).
I get this error message in FAIL.TXT: "The interface firmware FAILED to reset/halt the target MCU". And then STM32CubeProgrammer says "Error: No STM32 target found!" when trying to connect.
Maybe this issue relates to SB12, as the Nucleo-64 doc says: "SB12 NRST (target STM32 RESET) must be OFF if CN4 pin 5 is used in the external application".
So should I unsolder SB12? I prefer to ask, because AN5651 doesn't mention it.
Also, if I unsolder SB12, will I have to re-solder it for using the NUCLEO64-L476RG in the standalone way I'm used to?