usb cdc communication with high bit rate
hii every one
i implanted usb_cdc commination using usb port , and my question is how do i transmit data or receive with high bitrates lets say with 4 5 mbits , cause when i implanted the cdc-usb its just act like a serial port , and when i open the pc port there are standard bit rates like 115200 or 9600 etc , and i i am intersted to tarnsmite or recieve with higer bit rates how can i do that ? i be glad for help