USB-ECM Enumeration over USB for STM32L072
Using B-L072Z-LRWAN Board, I'm trying to Enumerate the USB Port as a Ethernet Adapter.(As Device not Host)
Thereby I integrated just the USB-ECM Stack provided by the STM32 itself.
I initially had issues with Driver, Post Following the Guide/Post from @tjaekel , i.e USB ECM demo - how to setup host? I used Belcarra USBLAN Driver, Though it got installed and is shown under Network Adapter, I see a Warning Sign for it

On Linux though, It gets identified as Android Tethering Device but doesn't show up on Wireshark nor Control Panel(Under Network).
So Below are my Issues:
- Is it Compulsory to Implement a Server Logic(LwIP, etc etc.) over the ECM Driver?
- Agenda of the Project is to USB Should be Enumerated as Ethernet Adapter on all OS Platforms, So Is ECM the Right Option?
- Can Someone Give me a Brief on, if I am to use ECM to achieve my agenda how and What are those Mandatory Components I need to include in the project.
- Keeping in mind the Board/Controller, STM32L072CZx, Wouldn't Implementing Server Logic use too much of memory? Just ECM Driver Integration alone uses 45.51% of RAM. As based on requirement we need RAM for other implementation too.