USB Type-C and Power Delivery on STM32G070RB
Hi,
We had an existing product using STM32G070RB powered by the USB Type-C and would like to detect the input source can provide the proper power delivery (15W, 5V, 3A).
I looked at the STM32 solutions for USB Type-C and Power Delivery document and noticed STM32G0x1 supports the build-in UCPD controller, but not STM32G0x0 series, is it correct?
If yes, then is there any example or suggestion to use STM32G0x0 series to detect PD source?
Thanks.
James Shih