Use NUCLEO-H745ZI-Q on-board STLINK-V3 as external debugger
Greetings,
I'm trying to use the STLINK-V3 debugger and programmer which is included on the NUCLEO-H745ZI-Q dev board to connect to external STM32. I have read https://community.st.com/s/question/0D53W00000OmiV6SAJ/nucleoh732zg-has-strange-new-stlink-part and that seems to be possible, someone suggested cutting SWDIO and SWCLK traces, but my board has the capability to completely disable the power to the STM32H745ZI by means of disconnecting the JP4 jumper which connects VDD to VDD_MCU which powers it. I have connected my wires to the CN5 connector (MIPI10 on STDC14 footprint) I have confirmed that I'm getting SWCLK and SWDIO signals from the STLINK-V3 but I'm constantly getting "Error: No STM32 target found!" in STM32CubeProgrammer.
The FW version of ST-LINK is V3J7M2.
Can anyone help me with this?
BR
Domagoj