Using more than 60 ST Link flasher on one PC with command line tool
My team has built up a complex test setup with about 72 ECUs of which all have an ST Link V2 connected to update all the controllers automatically.
With the help of an USB extension board they are all actively connected to the PC.
The issue is now, that the STM32_Programmer_CLI.exe (2.7.0) tool is only detecting exactly 60 of those connected flashers. The list output just shows 60 entries.
I access the flashers directly by their serial number. But it is only possible to access the ones directly, that show up in the list of 60.
The older ST Link Utility had the same issue.
I there any way to work around this issue?