Using Nucleo Board ST-Link for external STM32
I am using nucleo board, however, I try to use debugger on board for external board or stm32 microcontroller. I notice 6pin swd (cn6) on debugger. the first pin is VDD_targert. I followed up the wiring and connect to external target board. When I connect usb to pc, I found out pin 1(VDD_target) on CN6 doesn't have 3.3V. So If I would like to use this debugger for external target, I need power on target board or microcontroller to get this pin to have 3.3VDC, right?
Thank you for any help