Using X-Nucleo-LPM01A for measuring power consumption of NUCLEO-L432KC
Hello Everyone,
For a project, I'm using a NUCLEO-L432KC board and it is connected to external sensors, Tx, and Rx (which work with 4-5 V). I want to use an X-Nucleo-LPM01A to measure its power consumption.
Based on the NUCLEO-L432KC documents, I have to open SB9 and SB14, then NUCLEO-L432KC can be powered on by X-Nucleo-LPM01A then we can measure the board power consumption.
But there is a problem. if I use this method I can't use ST-LINK and USB to program the NUCLEO-L432KC board and I can't change some parts of the code. Each time, I have to solder them again, program the board, and then open the solder bridges SB14 and SB9.
Now the question is, is there any alternative solution?
I really appreciate your help