V2.J27.S6 Firmware
I have an ST-LINK / V2 Programmer with the number B 2018 33 containing Firmware V2.J27.S6, we are completely satisfied with it. The service needs in the field forced us to buy another ST-LINK / V2 with the number A2021 03 containing Firmware V2.28.S7.
Unfortunately, newly purchased devices cause problems and make it impossible to update programs. When trying to upload the update, the following error is displayed: "Programming error @: 0x08006648" Is it possible to upload the first version, which works fine? Is it still available somewhere ?? Unfortunately, it is no longer available on the website, the oldest one that can be downloaded is V2.J32.S7. Will the newer V2.Jxx.S6 be compatible ??