Skip to main content
Explorer
June 24, 2025
Solved

Vbat voltage supply to STM32U5G9NJ-DK1

  • June 24, 2025
  • 1 reply
  • 397 views

Hello,

We have procured STM32U5G9J-DK1 recently. We have to supply a voltage of 3.6V to its Vbat pin. Datasheet of the Microcontroller (STM32U5G9NJ) say that we can supply a Vbat voltage of 1.6V to 3.6V but schematic of this Discovery kit mentions that "The design supports a VDD_MCU at 1.8V only" (Ref MB1829 schematic of this Discovery kit). Also, whenever I configure any GPIO as output on this kit and Pull it high, it shows 1.8V only. So, my doubt is whether or not we can give 3.6V to Vbat pin. Should we restrict Vbat to 1.8V only ?

 

With regard,

Sudarshan Chaudhary

    This topic has been closed for replies.
    Best answer by QSHAO.1

    The VBAT can be setup to either 1V8 or 3.6V depends on your application. What implemented on STM32U5G9J-DK1 is an example of use case of same VBAT and VDD, however you are allowed to implement a VBAT with voltage in the range of VBAT = 1.65 V to 3.6 V. Thanks!

    1 reply

    QSHAO.1Answer
    ST Employee
    July 1, 2025

    The VBAT can be setup to either 1V8 or 3.6V depends on your application. What implemented on STM32U5G9J-DK1 is an example of use case of same VBAT and VDD, however you are allowed to implement a VBAT with voltage in the range of VBAT = 1.65 V to 3.6 V. Thanks!