Skip to main content
Visitor II
July 1, 2022
Solved

Virtual com port driver not properly installed

  • July 1, 2022
  • 1 reply
  • 2039 views

ST Link V3 SET is giving error due to virtual com port not installed in computer

    This topic has been closed for replies.
    Best answer by KDJEM.1

    Hi @KPate.6​ ,

    A similar question is already asked here.

    In the description of the STSW-STM32102 you can find:

    Virtual COM Port driver installation package for Windows® operating systems: 98SE, 2000, XP, Vista®, 7, and 8.x.

    Windows 10 does not require the installation of the Virtual COM Port driver anymore, as it is already built in.

    So, if you use a Windows® operating systems: 98SE, 2000, XP, Vista®, 7, and 8.x try to uninstall the driver and reinstall the last version.

    Kaouthar

    1 reply

    KDJEM.1Answer
    Technical Moderator
    July 22, 2022

    Hi @KPate.6​ ,

    A similar question is already asked here.

    In the description of the STSW-STM32102 you can find:

    Virtual COM Port driver installation package for Windows® operating systems: 98SE, 2000, XP, Vista®, 7, and 8.x.

    Windows 10 does not require the installation of the Virtual COM Port driver anymore, as it is already built in.

    So, if you use a Windows® operating systems: 98SE, 2000, XP, Vista®, 7, and 8.x try to uninstall the driver and reinstall the last version.

    Kaouthar