What is the pin for the user LED on UM2516?
Hello,
I am using an UM2516 (B-G431B-ESC1 Discovery kit) eval board with the STM32G431 microcontroller.
In the documentation is written:
"2 user LEDs: 1 green LED for 3.3 V level, and 1 red LED configurable by the user"
I want to use the red LED as visual feedback but i am not able to figure out on which pin of the microcontroller the led is connected. Its not mentioned in the official documentation under the chapter "STM32G431CB pinout for motor control" and not predefined in the program example of the eval board given.
Can someone help?
Is there a schematic for this evaluation board (discovery kit)?
Thanks for help in advance