What pins to power STM32F411CE with
I'm making a PCB for a project and am using the STM32F411CE (Otherwise known as the "Black Pill"). However, after spending many hours looking through the data sheet and searching online I'm still not 100% sure I understand how to power this board via battery. From my understanding the board does not have VDD and VSS pins. The only pins that I can tell are able to be used for power are 5v and 3.3v pins.
As per the datasheet, the board should not be powered by more than roughly 4v. That leaves me with just the 3.3v pins. Any other board I have used in the past has had VDD and VSS pins so I apologize if this is a silly question.
So my question is this, is it as simple as connecting 3.3v from a battery to the 3.3v pins and ground?
I am also a bit confused about whether I can power the board with 5v. As I stated earlier, the datasheet says not to exceed roughly 4v. However in the image below that source states there is a regulator that supports up to 6.0v.
So can I power the board with 5v after all?