When using an stlink V2-1 in external mode, can MBED drag-and-drop programming be used?
Several Nucleo boards come with an embedded stlink V2-1 which supports MBED programming by copying the firmware binary to a USB mass storage device. If the programmer is snapped off the board and put in to external mode, does this method of programming still work?
What about if the programmer is connected to a target with a larger flash memory than the board it was supplied with? In this case the USB storage device seems to remain the same size as the original target's flash and as such is not big enough to contain the larger firmware.