Where is .ioc file for Demo program for Nucleo board?
Hello Everyone,
1.
I have the Nucleo NUCLEO-H743ZI board.
I have powered it up and it performs as advertised.
I want to experiment and make some changes to the board programming.
I searched st.com site and found the file with all the demo software.
It was a huge 530+ megabyte Zip file.
I downloaded it and extracted it and found the files specifically for my Nucleo board.
I ran CubeMX and tried to "load" or "import" the project file for CubeMX.
As I understand this it, the CubeMX project file has an extension: .ioc
Unfortunately I cannot find it.
I used a file utility and searched hard disk for all of the files of all the demo software ( 1.1 gigabyte unzipped ) and there are no .ioc files at all!
Am I missing something?
Sadly, after reading various similar posts on this forum, I think that the Demo app was NOT developed with CubeMX so there is no file: .ioc
Question: Am I correct?
2.
OK, so given the Nucleo board, I can start over from scratch in CubeMX, and proceed to CubeIDE.
If for any reason, I want to re-establich the Nucleo with the original factory programming, I can accomplish that from within CubeIDE by loading the project as supplied by st.com in the above-mentioned mega-download.
Question: Again, am I correct in this?
Many thanks. This is great forum.
Best,
xst