Where to source a 5.08mm lead pitch crystal for Nucleo-64 board
I am finding it difficult to source an external crystal for the Nucleo-64 board (The F103RB). The footprint for the X3 crystal calls for a lead pitch of 5.08mm however this seems to be very uncommon. Most of the crystals out there specifiy a lead pitch of 4.88.
Now, looking at the user guide for the Nucleo-64 boards, it mentions a part from HongKong crystal, 9SL8000016AFXHF0, which is:
- Not useful for me as I want to be able to use a different frequency crystal
- The actual datasheet for that HongKong crystal specifies the lead pitch as 4.88mm :astonished_face:
Perhaps there an updated PCB design that has not made its way into the CAD resources section of the Nucleo-64 product page for the Nucleo F103RB?