Skip to main content
Graduate II
October 29, 2024
Solved

Which Nucleo boards can I use with X-NUCLEO-IKS4A1?

  • October 29, 2024
  • 2 replies
  • 941 views

I currently have a NUCLEO-F411RE, will I be able to use the X-NUCLEO-IKS4A1 expansion board with this or will I need another board?

 

Thanks

Nic

    This topic has been closed for replies.
    Best answer by AlexWEI

    hi 

    this sensor board is using the ardunio for connection, you can use nucleo/dk boards for the connection, the board mainly use the I2C/I3C connections. 

    2 replies

    Super User
    October 29, 2024

    It uses the standard Arduino headers.

    The whole point of those headers adopting the Arduino standard is that any other board which abides by that standard will work.

    AndrewNeil_0-1730206744507.png

     

    When in doubt, you can always check the schematics - they will be under 'CAD Resources' on the board's Product Page.

    The pinouts will also be defined in the board's User Manual.

    AlexWEIAnswer
    ST Employee
    November 13, 2024

    hi 

    this sensor board is using the ardunio for connection, you can use nucleo/dk boards for the connection, the board mainly use the I2C/I3C connections.