Which software to be used when using Nucleo board as a debugger to an external board as SWD?
I want the Nucleo board 303RE to act as a debugger for my external board. Two boards have an individual 3.3V supply so the ground has been made common. Other Hardware connections are below. Since CUBE IDE doesn't allow to flash Bin files using ST-LINK ....My question which software should I use to flash the bin file into the external board using Nucleo board's ST-Link. an anyone reply ASAP. Moreover when I select ELF file in CUBE IDE and debug my external board using Nucleo board's ST-LINK it gets into Hard fault handler....I checked the syntax of my code there is no issues with it....What should be the proper software and way to flash a bin file into external board using Nucleo's STlink and SWD?