Why am I getting only 1v from 3v3 when I unplug ST-LINK
When developing I'm using the ST-LINK to transfer my code to the stm32. All is well when it is plugged in but I'm only getting 1v from the 3v3 pin when I disconnect and run from usb. 5v is still 5v.
I've connected an hx711 with a load cell and also a 2x16 lcd but the lcd shuts down when unplugging the ST-LINK.
Does this mean I need an external power supply or can I use the 5v to get the 3v3?