Why can't I connect the ST-Link/V2 to my target board when the target is self-powered? (using the SWD)
If my board is not powered and the power is provided by the ST-Link, then I can program/erase all the time without issue. However for debugging it is not useful. As soon as I connect the power to the target I loose the connection.
Few things
SWDCLK and SWDIO are not used in the application
VCC is connected to ST-Link pin PIN 1 and Pin 19 thru a 10R
SWDIO is connected to ST-Link Pin 7
SWDCLK is connected to ST-Link Pin 9
GND is connected to ST-Link Pin 20
BOOT0 is pull down to GND
I did not used the ST-Link Utility, I used the STMCubeProgrammer or the STM32CubeIde.
Any clue why it does not connect to my STM32?