Skip to main content
Explorer II
June 24, 2023
Solved

why is LD3 (red power led) working with 3V3 input on NUCLEO-F072RB ?

  • June 24, 2023
  • 2 replies
  • 1773 views

I have this board (revision C-04) with ST-LINK removed (PCB cut off), so the power 3V3 is supplied from CN7. It works fine, but the red power led (LD3) also works. LD3 is, I think, connected to the 5V net, and 5V to 3V3 regulator should not be working but then why the LD3 is shining red?

    This topic has been closed for replies.
    Best answer by waclawek.jan

    > 5V to 3V3 regulator should not be working

     

    Many LDOs have built in reverse diode from output to input. 

    JW

    2 replies

    Super User
    June 25, 2023

    > 5V to 3V3 regulator should not be working

     

    Many LDOs have built in reverse diode from output to input. 

    JW

    meteAuthor
    Explorer II
    June 26, 2023

    I checked the datasheet, but I didn't see something like that. It makes sense, thanks.

    ST Employee
    June 28, 2023

    In this case, the SB2 should be removed to avoid any damage for LDO.