Why is voltage dropping too much in the 5V output Nucleo-STM32L432kc
Hello, Im trying to power this board and sensor with 30mA power consumption @ 5V with 5V output of the board.
What im noticing is the board is not capable of mantaining the voltage with this light consumptions. It starts at 4.7-4.8v with nealy 0mA consumption and when the sensor starts working (around 30mA consumption) the voltage drops to 4.2v and the sensor fails. Why is the voltage dropping this much when the board should be capable of providing 300mA output?