Why my MCU is not detected
In the picture:
pin 1 top left: VDD 3.3V
4 100n to GRND
14 to GRND
15 to VDD
16 to GRND
on their left 1µ and 10n F decoupling VDDA VSSA
pin 32 top right : VSS 0V GRND
pin 31 10K ohm to GRND
24 SWD clk
23 SWD dio
17 to GRND
top left and bottom right 100nF decoup. PWRS + the blue one 4.7µF
tried many combinations: with the reset on/off , boot0 on/off, swapped 23/34 ,
the ideMXcube and the standalone programmer wont see the MCU:
target not found,
ps: the red LED in ON .
my stlink v2 works in this setup with: another nucleo G4 and the generic "blue pill" fine.
Any help or suggestions ?
Thank you in advance.