Why the leg (pd8) is connected to ground in the schematics
can some one please tell me why is the schematics the pd8 is connected to gnd?
here is a picture of the schematics
can some one please tell me why is the schematics the pd8 is connected to gnd?
here is a picture of the schematics
Hello @YShko.1,
By default the PD8 and PD9 are used as GPIOs.
And when solder bridges SB29/SB30 are OFF, you can use PD8 and PD9 as GND and VDD as shown in the UM2324 and precisely in table 10.
But I notice a contradiction between the UM2324 and the schematic, Is it PD8 connected to GND or VDD?
I reported this issue internally.
Internal ticket number: 141998(This is an internal tracking number and is not accessible or usable by customers).
Kaouthar
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.